9/13/2016 3:17 PM | |
Posts: 28 Rating:
|
And here is the third and final install/setup log for the WinCC Comfort/Advanced. Thank you and Best Regards, John Blaser AttachmentWinnCC Comfort Install Log 3.zip (129 Downloads) |
9/14/2016 7:39 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
Hello, seems like there is not only the TIA Portal affected from the incomplete Data. You can try to reinstall the Automation Licence Manager. SIOS is the website here (Siemens Industrial Online Support)! https://support.industry.siemens.com/cs/ww/en/view/105825934 https://support.industry.siemens.com/cs/ww/en/view/106448872 Regards |
9/14/2016 2:46 PM | |
Posts: 28 Rating:
|
Hello All, Thank you for the responses, it is much appreciated. I uninstalled ALM and then began to try to reinstall it. I was given the following link to the ALM software: http://support.automation.siemens.com/WW/view/en/114358 The problem I have now is that whenever I try to reinstall ALM, I can't get it to load. I get a message saying 'Error 1327. Invalid Drive: E:\". What I can't understand is that I make sure that the installation location is: C:\Program Files\Siemens\Automation\Automation License Manager\" (which is the default link). I only see two log files generated last night when I tried to get the system to Run. I will attach them here. I will also try to put down the screen captures of what I did also. Again, thank you for all of the help. Best Regards, John AttachmentALM Install Logs.zip (111 Downloads) |
9/14/2016 2:47 PM | |
Posts: 28 Rating:
|
Hello All, Here is the attachment with all of the screen captures I did when I tried to install. Again, thank you for all of the help, it is much appreciated. Best Regards, AttachmentALM Install Screen Caps.zip (112 Downloads) |
9/14/2016 3:00 PM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating:
|
Start cmd with admin rights and subst e: "Your Install Folder here" and retry! |
~(‾▿‾)~ |
|
Follow us on