8/20/2009 12:24 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating:
|
Hi, Tips about PID V2.x, configured with STEP7 V12 could be found at (https://support.industry.siemens.com/forum/br/pt/posts/simple-sample-and-tips-step-7-pid-pid-compact-v3-tia-v19/309119/?page=0&pageSize=10#!#post1178234 ) Here are some tips about PID (FB PID_Compact): Together with the libary, there is a picture that shows how both block should be interconnected. 13Tuning that let very long times or aborts: |
Last edited by: Pegaia at: 5/20/2013 12:41 PMlink to pretunning conditions block Last edited by: Pegaia at: 2/28/2013 11:20 AMLast edited by: Pegaia at: 1/28/2013 7:02 PMLast edited by: Pegaia at: 1/7/2013 11:49 AMLast edited by: Pegaia at: 1/7/2013 11:46 AMLast edited by: Pegaia at: 1/3/2013 10:22 AMadd tip 13 Last edited by: Pegaia at: 5/28/2012 12:52 PMLast edited by: Pegaia at: 4/6/2011 1:04 PMOpen source PID Last edited by: Pegaia at: 4/6/2011 1:03 PMOperation with standard digital outputs. Last edited by: Pegaia at: 4/6/2011 12:50 PMLast edited by: Pegaia at: 4/6/2011 12:46 PMPID reset topic Last edited by: Pegaia at: 4/6/2011 12:43 PMInput PER filter Last edited by: Pegaia at: 2/8/2011 10:42 AMTips on error codes Last edited by: Pegaia at: 1/12/2011 6:32 PMLast edited by: Pegaia at: 1/12/2011 6:32 PMcorrection of typing error: sReti->sRet.i Last edited by: Pegaia at: 12/27/2010 12:45 PMlink for PID field simutation Last edited by: Pegaia at: 11/3/2010 3:09 PMreference to FAQ to limit PV Last edited by: Pegaia at: 6/15/2010 3:04 PMupdate of topic 7 Last edited by: Pegaia at: 6/11/2010 10:15 PMcorrect pg numbers of topic 7 Last edited by: Pegaia at: 6/7/2010 6:55 PMinclude topic 7 Last edited by: Pegaia at: 5/4/2010 10:01 PMincluding note 6. Last edited by: Pegaia at: 4/19/2010 2:40 PMLast edited by: Pegaia at: 4/19/2010 12:59 PMLast edited by: Pegaia at: 4/14/2010 12:55 PMLast edited by: Pegaia at: 8/24/2009 5:36 PMLast edited by: Pegaia at: 8/20/2009 12:27 PMLast edited by: Pegaia at: 8/20/2009 12:25 PMLast edited by: Denilson Pegaia at: 11/29/2023 11:08:59Denilson Pegaia |
|
This contribution was helpful to
33 thankful Users
|
4/6/2011 12:35 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating:
|
Hi, like descripted open, in 2.d, the FAQ " http://support.automation.siemens.com/WW/view/en/46163827“How can you prevent your S7-1200 PID Compact controller from going inactive in the case of a PLC power cycle and invalid process values?” give some tips to avoid a blocking, when are using the input "Input_PER". Sometimes, however, it is not possible connect the periphery directly to the PID. For the case of use the variable “Input” it is also necessary that the incoming values are float point valid values and inside of the input monitoring limits.The follow library has a version of theFAQ decrypted library to be used in this case. AttachmentPID_Compact FloatSignalFilter_lib.zip (2709 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
4/6/2011 12:40 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating:
|
If the PID Compact detects some fault in the controlled process (e.g. an invalid process value supplied), at security reasons, it goes to inactive mode. In this state the output of the PID stay not active. To bring back the PID to automatic operating mode it is necessary: 1 – Eliminate the fault cause. 2 – Make a change of the internal variable sRet.i_Mode from 0 to 3.
Attachmentreset PID.zip (2906 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
4 thankful Users |
Follow us on