2/21/2006 3:17 PM | |
Posts: 3149 Rating:
|
Hi concerning WinCC and optimizing performance there are already some faq /hints in your wincc online help, search for "diagnose" or "performance" => http://support.automation.siemens.com/WW/view/en/10538600 nemo |
2/21/2006 5:05 PM | |
Posts: 3149 Rating:
|
Hi, this objectshould containa Triggerslistwith all variables of this picture. Indeed using xxxWait-calls is not too good for your performance. nemo |
2/23/2006 4:12 PM | |
Joined: 12/5/2005 Last visit: 8/9/2021 Posts: 289 Rating:
|
Hi Salma. My problems are compounded by the fact that I'm not trying to debug one script. The animated objects areeach controlled by a script independently. The scriptsare very similar(in hind-sight, it would have been better to call a function to do the number-crunching). I've been working through one of the screens, and by a number of methods managed to get the initial update of the screen down to 15-20 seconds, but there is still a 7-10 second delay during which nothing seems to happen. I can try to post a copy of the screen here, if it helps. AttachmentMix-Tank.zip (650 Downloads) |
2/24/2006 9:43 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Can you try the GetTagWait suggestion and see if it makes a difference? |
2/24/2006 11:40 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
That's fantastic news ! Thanks for letting us all know. |
2/27/2006 9:47 AM | |
Joined: 12/5/2005 Last visit: 8/9/2021 Posts: 289 Rating:
|
I've gone through the screen I posted, replacing almost all of the script with the dynamic dialog connections. The update for that screen is less than two seconds, compared to the original 2 minutes. It's been a head-scratching day or two, but the result is worth it. I'm posting the new version so anyone who still has the last one can compare. Thanks for the help [:D] AttachmentMix-Tank2.zip (551 Downloads) |
3/9/2006 8:59 AM | |
Joined: 1/17/2006 Last visit: 5/20/2025 Posts: 800 Rating:
|
You can share the picture with us. Maybe we can help. |
3/10/2006 12:41 PM | |
Joined: 12/5/2005 Last visit: 8/9/2021 Posts: 289 Rating:
|
OK. Quick explanation - the Recipe screen has provision for up to 40 Recipes Each Recipe can have up to 16 steps, each with 13 variables (most are operator-inputs). When the screen is first shown, whenever the Re-Load button is pressed, or whenever a Recipe is selected (by clicking on the Recipe Name field just above the table), a script calculates the name of the tags required, and loads the values. AttachmentRecipe1.zip (563 Downloads) |
Follow us on