5/31/2012 5:33 PM | |
Posts: 6 Rating: (0) |
Hi everybody, I'm getting a very strange (and annoying) error on my S7-1200: About once a week my installation goes to stop mode. In the event log it says: Hardware configuration error - Removal of hardware component restricted - CPU switches to stop Event ID:16#02:4042 This happens while everything is running in a locked cabinet?!? so I don't think a hardware removal is even remotely likely I'm running a 1214 CPU firmware version 2.2.0 I have some screenshots as attachment (it's actually a .rar file instead of a .zip) If anyone has a solution (or even an idea to what is happening), it would be very much appreciated Tim
AttachmentNew folder.zip (225 Downloads) |
5/31/2012 6:27 PM | |
Joined: 9/19/2011 Last visit: 5/10/2024 Posts: 138 Rating: (33) |
For some reason I cannot download the file. What is your system configuration? |
6/1/2012 4:32 PM | |
Posts: 6 Rating: (0) |
CPU 1214 AC/DC/Rly 2x SM 1223 DC/Rly 3x SM 1222 Rly 24V power supply
|