8/2/2017 1:07 PM | |
Joined: 12/28/2016 Last visit: 12/22/2023 Posts: 364 Rating: (6) |
it says :- Ethernet Cable Use a "crossed" Ethernet cable for the connection between a PG/PC and an operator panel. If you use a "patch" cable, you need a switch in addition. Notes Operator panels with two "Ethernet interfaces" have an integrated switch. What is a crossed ethernet cable ? I tried connecting with Switch also but with the Switch the HMI was connected with Profinet Cable ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/3/2017 10:36:08 AMNew subject after splitting With kind regards... |
|