5/30/2015 10:36 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Davinator Sorry for delays response as I was at a project site. The first part ( Convert from Scout 4.3 to Scout 4.4 ) was smooth. However when I try to Migrate it into TIA portal, I get the following errors : Option package(s) missing in STEP 7 V5.4 SP5 or V5.5. Option package(s) SIMOTION missing in STEP 7 V5.4 SP5 or V5.5 I am not able to figure out which Option package is required List of installed softwares is attached. Thanks Navnag AttachmentInstalled_Softwares.xlsx (836 Downloads) |
There is no such thing as the last bug in a program |
|
Follow us on