1/11/2013 10:09 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
There is a way to controll which rtddl/dll is running or registered. Therefore you can use the Rtss Task Manager from Interval Zero which will be also installed when you install the Interval Zero RTX this must be the right website http://www.intervalzero.com/rtx-downloads/ the Interval Zero RTX is a free download If you want to have the Interval Zero SDK you have to pay for it |
1/11/2013 10:33 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
For the installation of the Interval Zero RTX you don't need any PAC-key. (i never need a PAC-key for this) |
1/11/2013 10:35 AM | |
Posts: 33 Rating: (0) |
Hi bigfoot, I have used RTXAnalyser (also from zero interval) on the PC and it came up with the results that i attached. I also attached screenshots from RTX5.1. Maybe you can see something on that. Greetings, Nico AttachmentRTX51.zip (843 Downloads) |
1/11/2013 10:41 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
Can you maybe send a screenshot a your SFB call for the RTDLL in your SCL-Source? |
1/11/2013 12:41 PM | |
Posts: 33 Rating: (0) |
Hi bigfoot, i've checked the rtdll wit dependency and found that not all files were in the correct folder. So i've adjusted this. But now i get another error (screen6). I've also added the code that calls the SFB (screen7). Is it possible that the problem is related to the OS? The previous one was 2000 embedded and now its XP. I'm setting up a machine with win2K now, and then im going to try it. The call of the sfb will not bring much info i guess, cause the string is loaded indirectly. But im sure that is has the following format: *RTSS:WinACTmSrv.rtdll Greetings, Nico AttachmentScreens.zip (716 Downloads) |
1/14/2013 9:49 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
Hello, a RTDLL ord DLL is an Output of an Visual Studio Project (VC++, VB, C#) which is created with the WinAC ODK Wizard. With the WinAC ODK Wizard you can create Visual Studio Project which create such an DLL/RTDLL file which can be run on an PC-based Controller. it is compressed and specially created that the PC-based Controller can read in interprete these files. The difference between RTDLL and DLL is that an RTDLL runs in the RealTime Kernel of Interval Zero. The big advantage of an RTDLL file is that is also runs if your windows turns into a blue-screen. I created for you an empty RTDLL with the ODK Wizard and tried it on my system. i registered the RTDLL and used the RTDLL in an simple STEP7 project which only makes a SFB65001 call. And everything works well. I attached the RTDLL for you. Why can't you register an RTDLL? Is there an error message? Have you installed all important software components? nice greetings bigfoot AttachmentC:\WinACTmSrv.zip (681 Downloads) |
Last edited by: bigfoot at: 1/14/2013 2:28 PM |
|
1/15/2013 9:15 AM | |
Posts: 33 Rating: (0) |
Hi, Im going to create a VM with win2K, maybe i can get it to work there. I'm setting it up now. Cant live with the fact that we did'nt solve it :) |
Follow us on