12/4/2014 4:44 PM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating:
|
Hello, I am trying to establish the mentioned connection WinCC7.2 and S7-1200 without success. I think I have done everything by the book: -added Simatic S7-1200, 1500 Channel, and added PLC's -set IP adresses for three PLC's -set access node to S7ONLINE for each of them -set PG/PC Interface to my local ethernet card, on TCP/IP protocol. This should be very simple but I don't get the connection. Just to mention, with S7 protocol suit and S7-300 everything is working fine on this computer, I usually make successfull connection in half of minute. Is there any trick I missed? I have WinCC7.2 update 7, SimaticNET, and that is it. Please see my screenshots attached. AttachmentWinCC S71200 problem.zip (215 Downloads) |
12/22/2014 9:35 AM | |
Joined: 1/22/2014 Last visit: 6/3/2024 Posts: 4 Rating:
|
I have similar problem, i cannot establish connection to s7-1200 with wincc7.2 // Simatic-net V8.2 Is there any parameter requirements in PLC side ? Also i have done all the previous mentioned steps bybanconi.
|
12/22/2014 10:19 AM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating:
|
Is this going to improve HMI capacity? |
12/22/2014 10:23 AM | |
Joined: 10/26/2005 Last visit: 6/10/2024 Posts: 284 Rating:
|
Hello, No, only allow free connections... exist in firmware v4. //Per |
12/24/2014 6:56 AM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating:
|
Were they both with firmware 4.0? The previous one and the new one? Best regards |
12/24/2014 7:52 AM | |
Joined: 1/22/2014 Last visit: 6/3/2024 Posts: 4 Rating:
|
No, the working one is with firmware 2.2, its older than 1200 with firmware 4.0. |
Follow us on