9/28/2017 1:21 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hello, you must install WinCC Runtime to get the Appl Entry in the Station Manager.
Christoph |
9/28/2017 1:25 PM | |
Joined: 3/20/2017 Last visit: 11/16/2023 Posts: 140 Rating: (2) |
WinCC runtime is installed |
9/28/2017 1:45 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hi, ok which Simatic Net Version you have installed, the WinCC Version is 7.4 ? Christoph |
9/28/2017 1:46 PM | |
Joined: 3/20/2017 Last visit: 11/16/2023 Posts: 140 Rating: (2) |
V14 |
9/28/2017 1:55 PM | |
Joined: 3/20/2017 Last visit: 11/16/2023 Posts: 140 Rating: (2) |
I have SP1 |
9/28/2017 1:58 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
in the screen i see only V7.4 but nothing about SP1? |
Follow us on