6/16/2022 4:37 PM | |
Posts: 71 Rating: (28) |
Hi Kramja, This usually hapens when you work with your panel's interface zoomed. As is said in the following FAQ: "make sure that the same scaling and the same font size are always set on the configuration PC and the visualization PC or operating device on which the PC Runtime is running". FAQ: Why are fonts and objects shown shifted on a PC Runtime system or operator panel?https://support.industry.siemens.com/cs/ww/en/view/13899072 Don't forget to rate if this post was useful!!! |
This contribution was helpful to1 thankful Users |