5/30/2022 2:21 PM | |
Joined: 4/1/2022 Last visit: 6/9/2022 Posts: 3 Rating: (0) |
WinCC OA - error when try to configure the ORACLE DB for RDB with way_of_backup set to datapump value - OS Linux CentOS 7, If I run the unix_install.sh with way_of_backup set to datapump value I get the error (see the log attached). What should I do to make the script work with way_of_backup set to datapump value (as recommended)? Thank you. AttachmentRDB_setup.txt (622 Downloads) |
Follow us on