2/5/2012 10:46 AM | |
Posts: 93 Rating: (0) |
Dear experts..
have attached a configuration.. kindly go through and tell of whether it is possible or not.. i have used s7 417h with cp443-6gk7 443-1ex20-0xe0..
i have assigned the mac address of the main cpu.. it is communicating without any problem.. but when i switch off the main cpu and the slave switches on, i am losing communication.. also tried am not able to establish s7- fault tolerant connection.,
i have only one cp1613 card..
please gimme a solution guys..
AttachmentPresentation1.pdf (59 Downloads) |