5/1/2020 4:04 PM | |
Joined: 2/5/2013 Last visit: 6/5/2024 Posts: 320 Rating: (74) |
Hi RenFlower, Try to install Hotfix 5 download for STEP 7 V5.6 and STEP 7 Professional 2017.link Which windows version/build installed on your PG/PC. Upload screenshot for same. Br, AmolG. |
Please rate it. |
|
5/5/2020 2:04 PM | |
Posts: 53 Rating: (0) |
Thanks. Sorry for the late reply. I have been busy working only had time to come back to thiis. I will download the hotfix and see how it goes. Thanks
|
5/7/2020 4:32 PM | |
Posts: 53 Rating: (0) |
Hello, I am unable to load video as the MAX is 3000KB. I made a short video of 20 seconds and its too big to load. Thanks |
5/7/2020 4:52 PM | |
Joined: 2/5/2013 Last visit: 6/5/2024 Posts: 320 Rating: (74) |
Hi RenFlower, Thanks for reply. I have faced same kind issue but installing hot fix resolved my problem. Have you checked that whether windos ver/build is compatible or not. Now if possible i will just suggest to install Step7 V5.6 SP2.The license for STEP 7 V5.6 / S7-GRAPH V5.6 / STEP 7 Professional 2017 will also remain valid with the SP2. 2.STEP 7 V5.6 SP2 download link
AmolG. |
Last edited by: Jen_Moderator at: 05/08/2020 07:42:17Optimized links. Please rate it. |
|