9/27/2010 6:52 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Hi, I assume by transparent you mean invisible. Under the properties of the button, change the Button Mode to invisible. Regards, Behnam www.sigmaprocess.ca |
9/27/2010 7:16 PM | |
Posts: 32 Rating:
|
There is no invisibility mode under the properties tab |
9/27/2010 7:39 PM | |
Posts: 32 Rating:
|
Found it..will give it a try. |
9/30/2010 3:43 PM | |
Posts: 32 Rating:
|
Thanks for the suggestion...will try. |
9/5/2022 11:36 AM | |
Joined: 10/2/2021 Last visit: 6/2/2023 Posts: 2 Rating:
|
Greetings, You can try the below mentioned steps for adding a transparent button in your WinCC Explorer. 1. Standard --> Windows Object --> Button 2. Fonts: You can leave it blank(No Space-bar needed) 3. Effects: Object Transparency-> 100, Global Shadow-> NO, Global Color Scheme-> NO, WinCC Style-> User Defined, Display Options-> Picture Only And then you can add any event as per your operation on this transparent button. For example I've added a pop-up screen on the button. If you do not have Object Transparency option in your version, you can go to STYLES-> Fill Pattern: Transparent(1), Line Weight->0 and then follow step 2 &3. Note: The blue outline in the video is just to show the placement of the button. Hope this solves your query Regards, Vivek Page AttachmentWinCC-Runtime - 2022-09-05 16-45-17(1).avi (738 Downloads) |
Last edited by: vivekPage at: 09/05/2022 11:44:04 |
|
Follow us on