3/22/2023 9:43 AM | |
Posts: 4 Rating:
|
Hi, thanks for the Post, i got same issue with HMI MP 377 screen, trying create and load recipes from mmc card, when i tried create a recipe it showing error, can say something about this. thanks nara. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/28/2023 04:17:07New subject after splitting |
|
3/23/2023 10:43 AM | |
Posts: 4 Rating:
|
Hi, |The main problem when tried read or write recipes, its not accessing and for saving new recipes also not happening, showing error aborted can some guide me on this please, see attachment for reference.
Attachmenthmi photos.docx (814 Downloads) |
3/27/2023 3:16 PM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello You do not have a connection to the PLC (all the ###) Then the system cannot read or write the recipe tags. Be sure that you connect to the real PLC or to PLC Sim and if you have eleminated the ### Then you will also be able to operate with the recipe funktions. Perhaps your PGPC Interface has not the correct settings. Check the basic FAQ: https://support.industry.siemens.com/cs/de/en/view/109748099 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on