1/9/2024 12:54 PM | |
Joined: 10/12/2023 Last visit: 1/16/2024 Posts: 2 Rating: (0) |
Hi, Where can i download a MSCEFile.dll from? None of these filesystems is working in my vb-script on windows ce 6.0. set fso = CreateObject("Scripting.FileSystemObject") I recieve error message ActiveX is missing. Thank you in advance for your help. Br Behnam ------------------------------------------------------------------------------------------ |
Last edited by: beazfa@gmail.com at: 01/09/2024 13:04:13Last edited by: beazfa@gmail.com at: 01/09/2024 13:05:15Last edited by: beazfa@gmail.com at: 01/09/2024 13:25:37Last edited by: Jen_Moderator at: 01/10/2024 09:36:41New subject after splitting |
|
1/11/2024 11:51 AM | |
Joined: 8/12/2021 Last visit: 9/24/2024 Posts: 324 Rating: (29) |
Hi! The "FileSystemObject" object is used with an RT Advanced. If you are using a screen, you will need to use FileCTL. There is an example that you can consult here. |
If this Information really helps, you could use the Rate function |
|
Follow us on