8/17/2024 1:49 PM | |
Joined: 1/10/2013 Last visit: 9/4/2024 Posts: 7 Rating: (0) |
Dear experts. I'm habing some issues with printing over TCP/IP form S7 1200. I'm using TSEND_C block to comunicate with printer. I have established communication and have printed from PLC. But the printer doesn't recognize the ESC/POS commands I send, it prints them as characters. I have sent the data as a single string, an array of strings, an array of char and array of hex with same results. Also, I have tested sending data with software from PC (Hercules, SendDataTool, PrinterTestTool) with the expected results, write the same code to PLC which results in printing all the commands as characters. I was wondering if there is a special way to send the commands to this printers, something like with Zebras printers, they use caret symbol before each command for it to recognice them as a commands. I'm using TIA PRO V19, 1214C FW V4.6 CPU and Epson TM-T20iiiL printer. Any help will be very appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/19/2024 06:46:46New subject after splitting |
|
Follow us on