5/11/2012 2:25 AM | |||||||||||||||||||||||||
Posts: 510 Rating: (117)
|
I don't know anything about the ProSoft device. In the TI World "X" and "Y" are inputs and outputs "WX" and "WY" are word inputs and outputs. The ".x" specifies the bit of the word from 1 to 16 I don't understand the mapping and the difference between the PB tag and the Programming tag. If you could explain it a little more maybe I can help you decipher your issue. billwest |
||||||||||||||||||||||||
5/11/2012 5:32 PM | |
Posts: 4 Rating: (0) |
Thank you for the reply, this may be more of a question of the S7 than the TI. The PB tag (tag sent over profibus) is the one that i'm trying to correlate. My question stems given the configuration parameters. How do I find which particular tags are being used. I think my confusion is mostly with the two different offsets. So if I'm trying to emulate QB50.0-QB50.7 from slave #21 does my configuration look like: DataInput ;Format for each 'mapping' line is ;offset,Node ,Area/Offset,Items,Type,CLX Tag Name 50,21,O/0,1,U16,Slv21_Out or ,21,O/50,1,U16,Slv21_Out or something different. I guess my question pertains to how data is organized in the S7. |
5/11/2012 9:04 PM | |
Posts: 510 Rating: (117)
|
I looked at the Prosoft manual and I interpret is to say So,21,O/50,1,U16,Slv21_Out should be correct |
5/11/2012 9:33 PM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
I am not sure you will get a fast resolution of your query either here or with Rockwell Forum. But you may always try for it. I have used many Prosoft modules, MNETR, MCMR, MCM,DNP etc with 1756 Control Logix Rack, but neither with Siemens. Prosoft technical support team is very good.I think you might already have the manual for the subject module, but still attaching it just in case you may need it. You may still wait for others to respond to your query, alternatively if you need urgent support, you may contact Prosoft at below number /email address. I am sure their tech support team have got the expertise to solve your query. Moreover, I do not think they would charge you anything for this. North America +1.661.716.5100, support@prosoft-technology.com
AttachmentAN-X-PB_UserManual.zip (548 Downloads) |
Last edited by: Lucky123 at: 5/12/2012 7:07 AMLast edited by: Lucky123 at: 5/12/2012 7:06 AM |
|
5/14/2012 6:41 PM | |
Posts: 4 Rating: (0) |
Thanks for the info, I've been trying to monitor tags without actually having a Seimens Master on the system and it's apparent that it's not going to work. So I'm patiently waiting for the TI to arrive. Thank you both for your help. -ebade |
This contribution was helpful to1 thankful Users |
Follow us on