7/15/2016 3:51 PM | |
Posts: 3 Rating: (0) |
Hi Bill, I have a SIMATIC TI545 PLC which was programmed with SIMATIC APT Software, the question in this regard it is possible migrate the program to S7 PLC progrmming software. Thanks a lot. Victor ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/18/2016 9:41:41 AMNew subject after splitting |
|
7/15/2016 4:30 PM | |
Joined: 9/27/2006 Last visit: 9/9/2024 Posts: 12282 Rating: (2682) |
Hello Victor; APT was a very advanced software for its time, and when siemens picked up the TI PLCs it evolved it to early forms of PCS 7. So it would be easier to look for a path to PCS 7 than to straight Step 7 programs. You could start with this discussion with some of our TI 505 programmers members: https://support.industry.siemens.com/tf/ww/fr/posts/102590/ There was even a migration path for APT programs to PCS 7/505 developped by Siemens: http://www.automation.siemens.com/w2/efiles/pcs7/migration/PABR0007.pdf Unfortunately there is no information available today on whether this PCS 7/505 OS still is provided; you would need to contact Siemens Support (use the Support Request link at the top of this page). Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 7/15/2016 4:30:36 PM |
|
This contribution was helpful to1 thankful Users |
7/22/2016 3:44 PM | |
Posts: 1 Rating: (0) |
Hello Victor, The link from Daniel's post has good information and some clear input from Bill about the difficulties in migrating directly from APT to Step7. Beside these programming difficulties, replacement of all the hardware can be extremely costly. Another post in the thread from Carlo outlines active support and continuing development of the 505 system and APT from CTI and FasTrak. Many APT and 505 users have found that this support relieves their need for migration and allows them to use those resources for more pressing projects. Robert |
This contribution was helpful to1 thankful Users |
Follow us on