2/21/2018 7:50 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi, See below: 1. Go to your motor block in CFC and open the properties of the block 2. Go to Messages under special properties. The External messages are defined under SIG4, SIG5 and SIG6 (External Message 1,2 and 3). If you connect a signal to I/O: ExtMsg1, you need to adapt SIG4 for example. One tip. If you follow above procedure, you will change the message for only that motor. If you want it to be changed for all motors in your project, you need to do the following: 1. Go to your Blocks folder of the AS project and find the FB number which corresponds to your Motor block (For example: FB1850 is MotL). 2. Right click on the FB block and select Special Object Properties->Message. You will find yourself in the same editor, only now you can adapt the messages for all the motor instances in your project. Good luck! |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/21/2018 8:34 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Can you show me a print screen? I don't know exactly what you mean...Can't you change the message or can you change it, but doesn't show up in the OS?\ |
If I could help you, you can use the RATE button. Thank you. |
|
2/21/2018 8:40 PM | |
Joined: 8/21/2017 Last visit: 7/5/2022 Posts: 75 Rating: (0) |
|
2/21/2018 8:41 PM | |
Joined: 8/21/2017 Last visit: 7/5/2022 Posts: 75 Rating: (0) |
|
2/21/2018 8:58 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
After an OS compile+Download OS you should receive the new messages. Did you do that? |
If I could help you, you can use the RATE button. Thank you. |
|
2/21/2018 9:08 PM | |
Joined: 8/21/2017 Last visit: 7/5/2022 Posts: 75 Rating: (0) |
I did. Hundreds of times haha it just doesn't show up |
2/23/2018 7:30 AM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hmm, I don't know exactly what is wrong with your project/settings, but you changed the message correctly. Maybe a OS full compile will solve the problem? Maybe something is wrong with your language settings? I see it is set on Brazil. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on