(0)| 3/16/2023 12:54 PM | |
|
Joined: 7/19/2022 Last visit: 1/13/2026 Posts: 436 Rating:
|
Hello Nnabi, First I would recommend that to make a copy of a WinCC project you do it from the Project Duplicator and not copying the project folder directly. As for what you say about not being able to start or stop a motor, if you look in the project the status of the start and stop variables you can see if there is connection with the controller and if they are acting and have the value that corresponds to them?
|
|
If this Information really helps, you could use the Rate function |
|
Follow us on