8/1/2024 6:58 AM | |
Joined: 4/15/2022 Last visit: 8/1/2024 Posts: 21 Rating: (1) |
Hello! I can't see any data blocks or tags. I can see the controllers basic information, but that's about it. And whenever I try to build a "Server interface" to try to combat this issue, the program crashes every time I try to compile or download it. (If I delete the "Server interface" under the "OPC UA communication" section, everything compiles and downloads again.) |
8/1/2024 9:24 AM | |
Joined: 3/11/2019 Last visit: 8/1/2024 Posts: 1538 Rating: (276)
|
Hi, i believe the crash goes into this direction: TIA Portal crash when compiling the PLC"Initial investigations have shown that there is a connection with a configuredOPC UA Server interface(OPC UA Client interface is not affected). If no OPC UA Server interface is configured in the project, the crash does not occur." There are also several topics in the "TIA Portal" subforum available. regards sancruz |
Feedback appreciated, please rate |
|
Follow us on