9/4/2006 3:13 PM | |
Posts: 122 Rating: (4) |
[:o]dear experts: i got questiones about the REPEATER show in "repeater"document.are there any influence to the segment1 line if one node got problem in the segment2 line? another question about the SWITCHES:the configuration of switches for process are designed as a ring(show in "switch2"document).but actually there is no connection betwween switch26 and switch27,so it is no a ring any more.i want to ask that are there any difference in communication between these two modes? thanks very much! AttachmentREPEATER.zip (882 Downloads) |
9/4/2006 3:22 PM | |
Posts: 122 Rating: (4) |
additional document[:P]
Attachmentswitch1.zip (858 Downloads) |
9/4/2006 3:24 PM | |
Posts: 122 Rating: (4) |
[:blush:]
Attachmentswitch2.zip (832 Downloads) |
9/10/2006 3:54 AM | |
Posts: 122 Rating: (4) |
i have tried to upload the attachment about the photo of switch but failed,i will try it again later. |
9/10/2006 9:50 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi Peters, It is possible to built a HSR {High Speed Redundancy} when you have a switch that can be the Redundancy Manager {RM}. It is also possible to built up two rings as standby link. The ring have to be built up so that the redundancy manager get on both sides of the ring physically the same ports. That ports could be electrical {100 MBit/s, 1GBit/s) or optical. The switches that could be redundancy manager are the older OSM, the X202-2IRT and the X204IRT (with RM firmware) and the X414-3E and the X408-2. Please read the handbook of the X400 serie carefully: SIMATIC NET Operating Instructions Industrial Ethernet Switches SCALANCE X-400 SIMATIC NET Configuration Manual Industrial Ethernet Switches SCALANCE X-400 From the X200-serie: Industrial Ethernet SCALANCE X-100 and SCALANCE X-200 Product Line And for the OSM: Industrial Ethernet OSM/ESM Network Management SIMATIC NET Industrial Ethernet OSM/ESM Because of the not clear situation, you might have now all posibilitys, please ask direct to the point with a powerpoint drawing or something what the exact (wished) built up is that you wish/have. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on