10/23/2021 8:35 AM | |
Joined: 9/15/2021 Last visit: 4/18/2022 Posts: 4 Rating: (0) |
root@iot2000:~/node-red# npm install node-red-dashboard npm WARN npm npm does not support Node.js v8.17.0 npm WARN npm You should probably upgrade to a newer version of node as we npm WARN npm can't make any promises that npm will work with this version. npm WARN npm You can find the latest version at https://nodejs.org/ npm ERR! URL is not defined npm ERR! A complete log of this run can be found in: npm ERR! /home/root/.npm/_logs/2021-10-23T06_31_50_931Z-debug.log how to update nodejs in iot2000 ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/25/2021 11:11:57New subject after splitting |
|
8/30/2023 2:04 PM | |
Joined: 7/26/2023 Last visit: 9/6/2023 Posts: 6 Rating: (0) |
I have the same problem because I updated npm. Are there any turnarounds? |
8/31/2023 8:38 AM | |
Joined: 4/28/2015 Last visit: 11/5/2024 Posts: 3345 Rating: (379)
|
Hi, to be able to install nodes again, I would re-install the Example image, use the installed versions and find nodes which are compatible with NodeJS v8. Unfortunately this can't be solved and the current image V3.1.17 is the final image for the IOT2040, because the product is on the phase "product cancellation". Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to2 thankful Users |
8/31/2023 8:42 AM | |
Joined: 7/26/2023 Last visit: 9/6/2023 Posts: 6 Rating: (0) |
Thank you! |
Follow us on