4/30/2024 2:26 PM | |
Joined: 5/6/2022 Last visit: 5/21/2024 Posts: 420 Rating: (83) |
Hi MartinT3, In principle, the main limitation is the panel itself, which has system limits that it can support. If you exceed the limits of the panel, the panel itself may cause problems, but if they are not exceeded, they should be supported by the Sm@rtServer as well. I don't know which HMI panel you are using but in all the manuals you can find these limits, I leave you an example of the Comfort Panels: "SIMATIC HMI HMI devices Comfort Panels: Scope of functions with WinCC" On the other hand, there are the following limitations for the Sm@rt options: "SIMATIC WinCC WinCC Engineering V16 – Options: Use and restrictions of Sm@rt Options" Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on