5/22/2024 8:20 PM | |
Joined: 2/25/2024 Last visit: 6/6/2024 Posts: 4 Rating:
|
Hello, I have been trying to use Openness to generate these System Tests and I really want to add the interface also through Openness. What I currently do is add a Server Interface manually under the OPC Ua Communication tab, and then start generating system test cases through openness. And then I download these new changes to the PLC SimAdvanced and then run the tests through Openness . Is there a better way to do this or is this the only way ? Currently through Openness this Server Interface does not have an “Import” feature, only an export, which is truly sad. I want to know your suggestions, or maybe you can give me new perspectives to deal with this problem.then run the tests also through openness. ( I want to use System Tests particularly because I have other SiL + I am unable to use Simatic Interface because my projects usually have a lot of nodes and to run a system test , it takes on average 10mins , absolutely pathetic when I have to run 100-200 test cases ) [snip] Thanks in advance ^.^ ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/23/2024 07:28:26New subject after splitting. Division of questions into separate topics. |
|
5/23/2024 7:30 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8192 Rating:
|
New question published by AutoGen_7594982 is split to a separate thread with the subject TIA Portal V18 crashes if the security settings for the PLC project are not configured correctly?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on