10/15/2024 7:20 AM | |
Joined: 1/4/2007 Last visit: 10/15/2024 Posts: 1147 Rating: (175)
|
Hello Raphael80s, 1. Check the alignment of the belt scale with 3 strings. See also the chapter 4.4.8 into the attached pdf-file. Check two rollers in front of the scale, and two rollers behind the scale (in sum: 5 rollers has to be aligned). The alignment has to be less than ± 0.8 mm. Put a little shim under the first and fifth roller, so that there is a little air gap between the string and the second … fourth roller. With a little air gap, you can see better the alignment. 2. Can you see in the BW500 integrator the correct belt speed? 3. How is the mv-signal, when the belt scale is unloaded? P940-01 (Cell A mV signal check)? P940-02 (Cell B mv signal check)? How is the mv-signal, when you hang in the two test weights? P940-01 (Cell A mV signal check)? P940-02 (Cell B mv signal check)? 4. Did you remove the transport lock of the belt scale? Best regards Siwarexi
Attachmentmanual_MSI_MMI_en.pdf (30 Downloads) |
Follow us on