8/27/2024 8:45 PM | |
Joined: 4/10/2023 Last visit: 11/1/2024 Posts: 2 Rating: (0) |
Was that issue solved? I have the same message. Didn't change anything. Even staring SIMATC WinCC Explore - "Logon failure: Unknown user name or bad password" when I'm trying to create new WinCC project. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/28/2024 08:49:27New subject after splitting |
|
8/28/2024 12:56 PM | |
Joined: 4/10/2023 Last visit: 11/1/2024 Posts: 2 Rating: (0) |
What I discovered so far: 1. Issue definitely related somehow to WinCC Explorer. It won't let me to compile OS project anymore because compiler can't open the project. 2. Tried to open another project on the same VM - same logon error. 3. I have a local copy of the same VM created a while ago. I archived project on network VM and retrieved it on my local VM and it let me to open OS project without any issues. 4. WinCC diagnose log saying after failed to open [see attached file] AttachmentPMStart.log.txt (149 Downloads) |
Last edited by: Moderator_Lan at: 08/28/2024 13:07:48Code attached |
|
8/30/2024 10:24 AM | |
Joined: 1/11/2019 Last visit: 11/4/2024 Posts: 790 Rating: (152)
|
Since it is sporadic issue and so many have not got into this issue you ca rise a service request from the below thread. |
Follow us on