10/11/2024 4:45 AM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 35 Rating:
|
HI, When i try to add profisafe address, it cannot identify Thank You, Baldeep |
10/11/2024 4:46 AM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 35 Rating:
|
Hi, The diagnostics buffer Shown Below Thanks, Baldeep |
10/15/2024 6:37 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, yes, a firmware update is possible in general but it depends on the module. Be aware: You mentoined to use a 6ES7136-6BA00-0CA0, but the photograph shows a 6ES7136-6BA01-0CA0. So be sure to use the correct firmware update for the module! The link below is the update for the BA01. Firmware update for ET 200SP F-DI 8x24VDC HFregards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
10/16/2024 8:58 AM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 35 Rating:
|
Hi, How do i update firmware on the hardware FDI Thanks, Baldeep |
Follow us on