11/5/2024 12:51 PM | |
Joined: 3/11/2019 Last visit: 11/6/2024 Posts: 1653 Rating: (303)
|
Hi, check the instruction DeviceStates. DeviceStates: Read module status information in an IO systemDepending on the mode given you can read information from the complete IO-system including states of the devices. Parameter MODEYou use the MODE parameter to read out status information. You can read out one of the following status information items for the entire PROFINET IO or DP master system:
regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
11/6/2024 12:13 PM | |
Joined: 6/9/2017 Last visit: 11/6/2024 Posts: 8 Rating: (0) |
Thank you for the help. That was incredibly precise and fast. |
Follow us on