11/5/2024 10:21 AM | |
Joined: 11/5/2024 Last visit: 11/6/2024 Posts: 2 Rating: (0) |
Good afternoon, colleagues! There was a problem like this: Attachmentproblem tia.zip (2 Downloads) |
Last edited by: Loluz at: 11/05/2024 10:32:14Last edited by: Loluz at: 11/05/2024 12:46:55 |
|
11/5/2024 2:24 PM | |
Joined: 7/19/2022 Last visit: 11/6/2024 Posts: 418 Rating: (70) |
Hello Loluz, It seems that you do not have the CPU version configured correctly in your project. You can see the CPU version from Device configuration > General You need to configure CPU with firmware V4.2 I recommend entering an unspecified S7-1200 and detecting the HW. Then upload the CPU. |
If this Information really helps, you could use the Rate function |
|
11/6/2024 5:44 AM | |
Joined: 11/5/2024 Last visit: 11/6/2024 Posts: 2 Rating: (0) |
Yes, you were right, the CPU version was 4.1, AttachmentProblem.zip (1 Downloads) |
Last edited by: Loluz at: 11/06/2024 05:44:46 |
|
Follow us on