1/27/2025 3:48 PM | |
Joined: 1/8/2025 Last visit: 1/30/2025 Posts: 7 Rating:
|
Hi all, Please, I need your help to fix PCS7 v9.0 SP1: CFC compilation error as shown in below picture. BR |
1/28/2025 2:24 PM | |
Joined: 3/14/2008 Last visit: 9/17/2025 Posts: 2217 Rating:
|
Hi, It looks like you are using an old AP library (which is fine). In order to use older libraries, you need to maintain the following:
The procedure is described in chapter 7.6 of the following manual: SIMATIC Process control system SIMATIC PCS 7 Software update V9.1 SP2 |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on