8/21/2006 2:21 PM | |
Joined: 12/28/2005 Last visit: 6/10/2007 Posts: 20 Rating: (2) |
You should do that , but first watch the software version of both and competability AttachmentS7200_MM4_USS_Connection.pdf (1010 Downloads) |
9/25/2006 1:37 AM | |
Joined: 4/6/2006 Last visit: 9/13/2024 Posts: 24 Rating: (2) |
Another option instead of purchasing the PC to MM440 kit is to get a RS-232 to RS-485converter. You can get it from B&B Electronics Part# 485SD9TB, their web site is www.bb-elec.com this provides a terminal strip going on the output of the converter so you can connect a 2 conductor cable to it. You connect the converter to terminal strip #29 & 30 on the drive. I have found this easier than the converter, also you still have the front operator panel. |
Follow us on