12/8/2016 10:46 AM | |
Posts: 40 Rating: (2) |
Which ip address is configured to your LAN interface on the pc? |
This contribution was helpful to1 thankful Users |
12/8/2016 1:20 PM | |
Posts: 11 Rating: (1) |
Hi Bermanu and Devguy, Thanks for pointing me in the right direction. I didn't get a ping. I managed to get it going with the attached settings. using this guide... http://www.howtogeek.com/howto/19249/how-to-assign-a-static-ip-address-in-xp-vista-or-windows-7/ Posted it here so it may be some help to others. The note at the bottom of page 16 could do with expanding a bit to let us newbs know how to check subnet and change settings if needs be. Thanks Again. Richard P.s. I'm used to being spoon fed with the S7-1500 / TIA Portal :) |
Follow us on