8/2/2017 10:13 AM | |
Joined: 10/26/2011 Last visit: 10/28/2024 Posts: 762 Rating: (191)
|
Hello, there are two application examples available in the Siemens Industry Support: SIMATIC PCS 7 in the mining industry (demo project)https://support.industry.siemens.com/cs/ww/en/view/81723640 The demo project contains multiple process screens that are intended to clarify the project using the example of a processing plant (e.g., for copper). In the "Crushing" area, the function of a crusher, including the removal of the raw material by conveyor belts, has been visualized. This plant area is configured for the demonstration of MinAS. The remaining screens are static and do not have an individual function.
SIMATIC PCS 7 in Mining (Video) The video "SIMATIC PCS 7 in Mining" gives you an overview of the features and advantages of PCS 7 being utilized in the mining industry through the following topics:
|
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to2 thankful Users |
Follow us on