1/26/2018 10:13 AM | |
Joined: 3/26/2009 Last visit: 8/27/2024 Posts: 29 Rating: (2) |
I have a very similar problem. I want to read the LADDR of an input. But I have to use the IO2MOD function inside an FB which has the input as an IN variable. With the function GetSymbolName i can read the signal name from the IN variabel as a string, for example "DI2". I can use the IO2MOD function with the symbolic name of the input, but I cannot use the string i read. So is there any way to use a string as a symbolic name input to IO2MOD? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/26/2018 2:51:53 PMNew subject after splitting |
|
Follow us on