10/23/2020 9:07 AM | |
Joined: 5/12/2006 Last visit: 8/7/2024 Posts: 22337 Rating:
|
Hi, and which step7 Manager version you use? Latest versio is 5.6 SP2 Upd3 |
11/16/2020 10:16 AM | |
Joined: 3/11/2019 Last visit: 8/7/2024 Posts: 1546 Rating:
|
Dear paul.mnt, even if it works again in the meantime, the latest version is V5.6 + servicepack 2 + hotfix 5. As i can see on the screenshot, V5.6 with servicepack 1 is installed. Maybe this helps if the message is shown again. regards. STEP 7 V5.6 SP2 / S7-GRAPH V5.6 SP2 / STEP 7 Professional 2017 SR2 Trial DownloadDownload Hotfix 5 STEP 7 V5.6 SP2 / STEP 7 Professional 2017 SR2 |
Last edited by: sancruz at: 11/16/2020 10:18:51Feedback appreciated, please rate |
|
This contribution was helpful to
2 thankful Users |
12/15/2021 10:00 PM | |
Posts: 1 Rating:
|
I had same issue and this totally helped. thanks a lot. |
8/9/2023 8:05 AM | |
Joined: 1/24/2023 Last visit: 5/13/2024 Posts: 2 Rating:
|
Hello, I have the same error, but I can't install version 5.6 sp2 (I have 5.6 sp1) because link is "controlled" and my registration inquiry is still being processed. link: https://support.industry.siemens.com/cs/de/en/view/109773842 Is there other way to solve it ? Or to expedite registration ? What should I do? |
Last edited by: Jen_Moderator at: 08/09/2023 10:28:40Link optimized. |
|
Follow us on