6/30/2023 2:31 PM | |
Joined: 5/6/2022 Last visit: 10/4/2024 Posts: 461 Rating: (90) |
Hi Hairyvelcroman, After reviewing the capture and the information in the post, tell you that the RC also has a number of tags associated with it, but you don't indicate it in the post. It is likely that you exceed the tags that you have licensed. And for the part of having another backup server it would already be the redundant configuration with a redundancy license. Best regards! |
If this Information really helps, you could use the Rate function |
|
7/4/2023 9:54 AM | |
Joined: 4/28/2015 Last visit: 9/5/2024 Posts: 9 Rating: (0) |
Hi - Licences are attached from the old server and the new server. I have a RC licence that I will move over to the new server when we migrate over to the VM machinery. I am currently using a RT licence whilst setting things up. -TCP/IP tags are 254, and the OPC tags are 4573. This is the 4827 issue that I am having on the Licence Analysis capture -We are using v7.5,SP2, upd11 on the new server. We haven't got redundancy. I was planning on just using the RT licence that we have on the back up server just in case. In an emergency, we can spin this up, and not care about configuration, so we could just use the RT licence for this. We do need a second 7.5 server licence as we currently only have one. Thanks Nathan AttachmentForum response.pptx (277 Downloads) |
Last edited by: Hairyvelcroman at: 07/04/2023 10:06:52 |
|
10/4/2024 8:33 AM | |
Joined: 7/30/2024 Last visit: 10/4/2024 Posts: 183 Rating: (3) |
New question published by rasoolsharifi1 is split to a separate thread with the subject Best license for this project. Best regards |
Follow us on