10/2/2024 11:29 AM | |
Joined: 5/27/2024 Last visit: 11/6/2024 Posts: 26 Rating: (0) |
Can I use the 6ES7870-1AB01-0YA0 dongle with the CP-341 for Modbus RTU Slave communication in an S7-300 system using TIA Portal V13? What are the differences between the 6ES7870-1AB01-0YA0 and the 6ES7870-1AB01-0YA1? Do I need additional software for this, or is only the hardware dongle required? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/02/2024 11:49:25New subject after splitting |
|
10/2/2024 11:57 AM | |
Joined: 7/9/2015 Last visit: 11/6/2024 Posts: 4019 Rating: (601)
|
Hi, 6ES7870-1AB01-0YA0 contains License for Modubus Slave and Software/Documentation. It´s for CP341 / CP441-2. 6ES7870-1AB01-0YA1 contains also License but no Software / Documentation. Please check this manual for detailled informations: SIMATIC S7-300/S7-400 Loadable Driver for Point-to-Point CPs: MODBUS Protocol, RTU format, S7 is SlaveYou need FB80 - so check chapter commissioning the FB... Regards Towome |
Last edited by: Towome at: 10/02/2024 12:00:15
|
|
10/3/2024 4:45 AM | |
Joined: 5/27/2024 Last visit: 11/6/2024 Posts: 26 Rating: (0) |
Thank you. |
Follow us on