2/14/2022 3:24 AM | |
Joined: 1/14/2022 Last visit: 3/3/2024 Posts: 21 Rating: (0) |
I am looking for help on a project I am working on, it is a pneumatic sprayer application, there are 9 pneumatic solenoids controlled from relay outputs on the LOGO I am calling them zones 1-9. The project parameters are: zones 1-9 are to run sequentially for 10 minutes periods from 4:30am to 4:30pm starting with zone 1 and ending with zone 9 repeating zone 1-9 for 10 minutes each until 4:30pm. zones 1-9 10 minutes each = 90 minutes total cycle repeating the cycle for 12 hours the only way I can figure out how to do it is using multiple 7-day timers using Cams 1-3 per relay output To achieve a repeating timing sequence for 12 hours I will need three 7-day timers using all Cams per timer. I was going to create a web page to edit the timers, but I will exceed 65 VM mappings for this solution. I am looking for any idea of any other solutions besides a 7-day timer that could be used to achieve the goal. I have attached my current project file. Thank You AttachmentSprayer timming.zip (540 Downloads) |
Last edited by: userB at: 02/14/2022 03:26:12Last edited by: userB at: 02/15/2022 05:48:13 |
|
2/14/2022 5:37 AM | |
Joined: 12/18/2014 Last visit: 5/29/2024 Posts: 33124 Rating: (4089)
|
Maybe the solution in attachment is what you want ... For testing is the pulse time of the pulse generator 3s. You must change it to 10 minutes. AttachmentValve_intervall_FS4.zip (482 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on