3/25/2015 4:06 PM | |
Posts: 4 Rating: (0) |
You can buy it from any Siemens Rep note: the new design 353 design B has an MMC card inside who store the configuration JMA |
5/25/2016 12:32 AM | |
Joined: 10/3/2006 Last visit: 10/6/2024 Posts: 44 Rating: (0) |
Hi, I already have the cable needed. (I think) I have a problem using iconfig to connect it to the 353 loop controller. I connected my cable from the serial port (com1) of my laptop to the bottom front part of the 353 loop controller as shown in the picture attached. Based on the software manual, I have to select from 353DIRECT, 353MODBUS, and 353ICI320. My logic says that I should connect to 353DIRECT, but the driver is not present in the software that I have. See attached pictures. Can you help me upload the configuration from this device to my laptop?
Attachment353_pics.zip (702 Downloads) |
Last edited by: jenie at: 5/25/2016 12:33:52 AM |
|
3/30/2017 8:25 PM | |
Posts: 1 Rating: (0) |
Is there software available for the Siemens 353? I tried the link and its looking for a Step 7 product that doesn't work. |
Follow us on