4/15/2021 11:51 AM | |
Joined: 1/4/2021 Last visit: 8/9/2025 Posts: 17 Rating:
|
The parameter DATA_TYPE, START_ADDRESS etc. are input/output parameters as in the local variable of Fb shows . i am still not able to catch it . in logic it seems it data is coming momentary but again overwritten to 0 value again . The MODBUS_PARAMETER_PN Db & CONTROL_DATA DB screen shot attached........ AttachmentPics.zip (946 Downloads) |
4/22/2021 10:30 AM | |
Joined: 1/4/2021 Last visit: 8/9/2025 Posts: 17 Rating:
|
The file size too big , it can't upload here , So I am sharing the We transfer link , Please load the project . [snip] inside this project FC -900 is containing the code. AttachmentUtility_share.zip (872 Downloads) |
Last edited by: Jen_Moderator at: 04/22/2021 12:45:19Removed link and added file as an attachment. |
|
Follow us on