8/24/2023 11:52 AM | |
Joined: 8/18/2014 Last visit: 9/15/2025 Posts: 73 Rating:
|
I did this back in 2014. I startet with the linked code How to program ATLAS COPCO - 13246 - Industry Support Siemens Now i am on PCS7 V9.0 Sp3 and i dont know if it would be helpful to upload my modified function blocks. It works ok but the CAN communication logic is horrible. Other compressors (i.e. KAESER) have proprietary PB or PN interfaces which is way easier to handle. |
Last edited by: JOMAK at: 08/24/2023 11:58:32 |
|
9/1/2023 5:14 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello,
this isn't only CAN bus, they have compressors also with PN or PB without problems, all depends to actual type of device. Therefore is there some Gateway to better bypass hard work with CAN bus and have to do only control system programming - all managed via control byte/other mechanism, that Gateway then solves internally. This is simply best option in this case to my opinion. You need to do tests and have good experience with some similar networks previously. |
With best regards... |
|
Follow us on