2/21/2024 10:38 AM | |
Joined: 4/9/2021 Last visit: 4/22/2024 Posts: 4 Rating: (0) |
Hello everyone. I'm trying to install TIA Portal V19 on my laptop but everytime installation process goes wrong. I have TIA Portal V16 on my laptop which is running correctly. I had also TIA Portal V17 but I unistalled it before trying to install TIA Portal V19 because my projects are on V16 (I never done migration, and I would like to do now from V16 to V19). My OS is Windows10 Pro (22H2 Version), processor is Intel(R) Xeon(R) CPU E3-1535M v5 @ 2.90GHz with 16GB RAM. Installation settings are standard. I also tried to install without Windows Firewall but nothing changed. Attached you can find log file of last installation. Please help me! Thanks AttachmentSIA_STEP7_S7FPLUS_WINCC_V19@24-02-21_11-16-53_summary.txt (573 Downloads) |
2/21/2024 3:22 PM | |
Joined: 5/6/2022 Last visit: 10/17/2024 Posts: 469 Rating: (94) |
Hi marcornc, What version of TIA Portal exactly do you have installed or/and did you have installed (Basic, Advanced, Professional, Unified...)? And from what I see you have V16, you deleted V17 and now you wanted to install V19. I'm telling you this because you may be having problems possibly due to SQL if it is Professional/Unified. If so, even if you delete the software, it is possible that some instances remain. You can try to eliminate these ("Upgrading WinCC Professional & SQL Server"). If you cannot remove it completely, you should still start from a clean image or install it in a virtual machine. Can you clarify what you have installed? Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on