10/2/2024 9:00 PM | |
Joined: 3/25/2024 Last visit: 10/14/2024 Posts: 3 Rating: (0) |
Hello everyone, I have a S7-1500, 6ES7511-1AK02-0AB0, that I need to make a copy of the program which resides on the PLC itself. What I have attempted to do is,
Midway through the process, I get a message that says "Totally Integrated Automation Portal has encountered a problem and needs to be closed." The software then became unresponsive, and I have to kill the software in Task Manager Process. I tried the same step in different Windows OS such as Windows 7 and Windows 10 but nothing changes. I get the same message, and the software become unresponsive. I tried to upload the PLC program only but still no avail. I attached the crash log in the post for reference. I really appreciate if anyone can point me in the right direction. Thank you for your time. Attachment824bdaaf-50e0-4a8e-a536-07113aa4fd4a.zip (11 Downloads) |
10/2/2024 9:45 PM | |
Joined: 7/7/2010 Last visit: 10/18/2024 Posts: 15326 Rating: (2432) |
Try TIA Portal V13 SP2 - with latest update. |
science guy |
|
10/3/2024 11:23 AM | |
Joined: 5/6/2022 Last visit: 10/18/2024 Posts: 470 Rating: (94) |
Hi Luanonsemi, Regarding uploading a project, I'm sharing a FAQ that may be of interest to you: "What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?" However, the problem as you mention is due to a crash. Could you please attach the crash by saving it as .dr to see if there is information with that file? Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
10/4/2024 3:05 PM | |
Joined: 3/25/2024 Last visit: 10/14/2024 Posts: 3 Rating: (0) |
I tried again using TIA Portal V13 Pro. SP 2 Update 4 but I still get the same issue. |
10/4/2024 3:08 PM | |
Joined: 3/25/2024 Last visit: 10/14/2024 Posts: 3 Rating: (0) |
How do I save the crash file as .dr? When it prompted me with the crash message it did not give me an option to save the file in a different extension. I attached the latest crash log for reference. Attachmentf6eb2747-bfc2-4cbd-9c6a-f24764f6a66d.zip (12 Downloads) |
Follow us on