2/16/2017 6:21 PM | |
Posts: 158 Rating:
|
I figured. So bascially I need to make one of the masters a 2nd slave. Just thought I'd check. Thanks |
2/16/2017 6:27 PM | |
Posts: 158 Rating:
|
FS04 |
2/16/2017 6:38 PM | |
Joined: 12/18/2014 Last visit: 9/6/2025 Posts: 35928 Rating:
|
Here a small example. Don't Forget: You must the slave-LOGO! set into slave modus. Tools > Transfer > Configure Master/Slave Mode AttachmentTest_2_Master_1_Slave_0BA8.zip (395 Downloads) |
2/17/2017 7:55 AM | |
Joined: 12/18/2014 Last visit: 9/6/2025 Posts: 35928 Rating:
|
In the examples in the attachment, I show you how to send signals from the new 0BA8 to the already existing 0BA7 and send them from the two 0BA7 to the 0BA8. All three LOGO!s are masters. The notes include: 1 x UDF HighByte 1 x LSC file (15_bits_of_a_0BA7_send_to_a_partner.lsc) as sample file for the use of the two UDFs. 1 x MNP file (3xMaster_1x0BA8_2x0BA7.mnp) as an example project for networking the LOGO!s. AttachmentExample.zip (350 Downloads) |
2/17/2017 9:11 PM | |
Joined: 12/18/2014 Last visit: 9/6/2025 Posts: 35928 Rating:
|
The next problem: UDFs only can be programmed in FBD, can not convert to LAD. |
2/17/2017 9:31 PM | |
Posts: 158 Rating:
|
What if I use all 0BA8? I should be able to do it like you did in your sample "Test_2_Master_1_Slave_0BA8" yes? |