Industry Online Support
Technical Forum
7/17/2024 10:47 AM | |
Joined: 5/30/2022 Last visit: 7/17/2024 Posts: 553 Rating: (94) |
Hi BELAL 399, It is not possible to restore a backup made by prosave between two different screens. You must first have the original OP 37 program. This screen, I seem to remember, is only programmed in protool so you would first have to do the migration to wincc flexible: SIMATIC HMI WinCC flexible 2008 WinCC flexible 2008 Migration and then from wincc flexible to TIA Portal: Or create from scratch the program already in the current screen.
|
If this information really helps, you could use the Rate function. |
|
Follow us on