(0)| 2/13/2025 12:22 PM | |
|
Joined: 4/7/2024 Last visit: 11/2/2025 Posts: 5 Rating:
|
Hello, Can someone help? I have a problem with my S5 115 CPU 944 all the Fault LEDs and status LEDs are constantly ON; What is strange is that both the ST and RN LEDS remain on regardless even when I toggle the Run and Stop Switch.. The status indicator LEDs on the power supply unit are all ON; I have removed all I/O cards from the central rack but all the LEDs on the CPU remain ON; The CPU cannot communicate with the PG; suspect there could be a problem with the CPU or other I/O device. My technical team has informed me that one Input module blew up upon restoration of power to our control panel.; we do not have any spare CPU or IO that we can swap as part of our diagnostics.. Any ideas out there? ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_7836103 at: 02/13/2025 12:26:48Last edited by: Moderator_Lan at: 02/13/2025 12:35:56New subject after splitting |
|
Follow us on