1/30/2017 2:22 PM | |
Posts: 5 Rating: (0) |
Hi bergmanu, thanks for your fast answer, but it still doesn´t work. In the direction "IOT2000 Release" is nothing to select. |
1/31/2017 11:12 AM | |
Posts: 5 Rating: (0) |
Hi, here is the consoloutput after the build process (attachment). What does the error message mean? |
1/31/2017 11:20 AM | |
Posts: 71 Rating: (16) |
Hello schmidpa, please have a look at this thread: https://support.industry.siemens.com/tf/ww/en/posts/build-error-for-the-example-application/160267/?page=0&pageSize=10 |
2/21/2017 12:59 PM | |
Posts: 71 Rating: (16) |
Unpacking the archives creates links on the file system. Those are not created properly if 7zip is run without administrator rights. |
3/23/2017 8:18 PM | |
Posts: 1 Rating: (0) |
Hello, the example in the Getting Started shows how to programm the IOT2000 with C/C++. Is it also possible to use other languages like C#? |
4/9/2017 7:14 PM | |
Posts: 2 Rating: (2) |
Hello, I installed the Getting Started on my IOT200, too, and want to start my exercises. But I cannot find any documentation how to address the IOs. For example: where is documented, that the USER led is addressed via mrcc with number 13? And where is documented, how to address the USER button? I found the documentation about the mrcc at http://iotdk.intel.com/docs/master/mraa/index.html but I could not find any device specific information there. Best Regards, barteldan2 |
This contribution was helpful to1 thankful Users |
4/11/2017 10:05 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi, that the USER LED is pin 13 is described in the Getting Started Document. There are several posts about the User Button. For example here: https://support.industry.siemens.com/tf/ww/en/posts/how-can-the-status-of-the-user-button-be-queried/152949/?page=0&pageSize=10 The assignment of the other GPIOs could be found here: or you can use this picture for example. Best regards! |
Last edited by: bergmanu at: 4/11/2017 10:05:40 AMNot working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on