9/12/2011 2:41 PM | |
Posts: 7 Rating: (0) |
hi, i have STEP7 10.5 SP1 regards |
9/13/2011 12:49 PM | |
Posts: 25 Rating: (0) |
Impossible to open ? it's a zip-file, did you extractit ?? I was able to open it. My question ; I tried theexample on my home-PC & PLC and from the 1st try, I was ableto view the data log files. When I added the example to myreal program (other PC and PLC), I usedother markers and markerwords, but I suppose it's working because I see the nr Created increase when I do a DataLogCreate and the same when I do a DatLogWrite.So I suppose the logging is working. When I go to theinternet explorer, I get a datacommunication error instead of that screen of the S7-1200 CPU Webserver. My IP-addresses are 9.0.0.1 for the PC and 9.0.0.10 for the PLC and I enter http://9.0.0.10/ in my internet explorer. What is the problem here ??? If I close the file with a DataLogClose, it doesn't help. Is it necessary that the siemans-software is open and the a certain screen is activated or other preconditions ? Has it something to do with the IP-address starting with 9 instead of 10. Is it because it's another type of ethernet-port??? bart I found the answer (stupid) : enable the webserver in the properties of the configuration of the PLC |
Last edited by: BSALV at: 9/13/2011 3:04 PM |
|
Follow us on